2026-05-11 2:46 PM
Hello everyone, I have a custom PCB with an RFM69HCW and an STM32L011G4U6, I'm stuck, transmission and reception work fine, but if I want to add an ID, it gets stuck, here are my two INI files, sorry for my English.
void RFM69_Init_RX(void) {
uart_print("=== RFM69 CAPOT RX INIT (868MHz) ===\r\n");
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_Delay(10);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_Delay(50);
RFM69_WriteReg(0x01, 0x04); // Standby
HAL_Delay(10);
// === Fréquence 868 MHz ===
RFM69_WriteReg(0x07, 0xD9);
RFM69_WriteReg(0x08, 0x00);
RFM69_WriteReg(0x09, 0x00);
RFM69_WriteReg(0x11, 0x7F); // Puissance max
// Configuration Paquet
RFM69_WriteReg(0x02, 0x00); // Packet mode
RFM69_WriteReg(0x03, 0x1A);
RFM69_WriteReg(0x04, 0x0B);
RFM69_WriteReg(0x2F, 0xAA); // Sync Word
RFM69_WriteReg(0x30, 0x55);
RFM69_WriteReg(0x37, 0x00); // Pas d'adressage
RFM69_WriteReg(0x38, 9); // Payload Length = 8 octets (suffisant pour "arm" et "off")
RFM69_WriteReg(0x3C, 0x80); // Clear FIFO
RFM69_WriteReg(0x01, 0x10); // Mode RX
uart_print("CAPOT RX READY - En écoute (arm/off)\r\n");
}
and : void RFM69_Init_TX(void) {
uart_print("=== RFM69 TELECOMMANDE INIT (868MHz) ===\r\n");
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_RESET);
HAL_Delay(10);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_3, GPIO_PIN_SET);
HAL_Delay(50);
RFM69_WriteReg(0x01, 0x04); // Standby
HAL_Delay(10);
// === Fréquence 868 MHz ===
RFM69_WriteReg(0x07, 0xD9);
RFM69_WriteReg(0x08, 0x00);
RFM69_WriteReg(0x09, 0x00);
RFM69_WriteReg(0x11, 0x7F); // Puissance maximale
RFM69_WriteReg(0x02, 0x00); // Packet mode
RFM69_WriteReg(0x03, 0x1A); // Bitrate
RFM69_WriteReg(0x04, 0x0B);
RFM69_WriteReg(0x2F, 0xAA); // Sync Word
RFM69_WriteReg(0x30, 0x55);
RFM69_WriteReg(0x37, 0x00); // Pas d'adressage
RFM69_WriteReg(0x38, 8); // Payload Length max (on met 8, c'est suffisant pour "arm" et "off")
uart_print("TELECOMMANDE RFM69 Initialized\r\n");
}
2026-05-12 7:48 AM
@fanfan6966 wrote:I have a custom PCB
You'll need to show the schematic, then - see: How to write your question to maximize your chances to find a solution
@fanfan6966 wrote:with an RFM69HCW
You mean this: https://www.hoperf.com/modules/rf_transceiver/RFM69HCW.html ?
That's not an ST product, so you need to go to HopeRF for support with that:
https://www.hoperf.com/contact/
wrote:transmission and reception work fine
So your basic comms & connections must be OK; therefore unlikely to be anything to do with the STM32 itself.
@fanfan6966 wrote:if I want to add an ID, it gets stuck,
What, exactly, does "stuck" mean here ?
Where, exactly, does it get "stuck" ?
What debugging have you done to find why it's "stuck" ?
2026-05-12 2:51 PM
Hello, I know the problem isn't the STM32. When I say it's blocked, it has nothing to do with the STM32, but rather the code. By adding an ID, I no longer have any communication. The manufacturer doesn't respond, nor does their help site. I just thought that someone had probably programmed this type of module using STM32.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.