Skip to main content
Associate II
May 8, 2025
Solved

8-bit DCMI Camera Reference Design?

HI, I am MURALI SELVAM from India, I need reference design for Below given part number. I want DCMI Camera Interface 8-bit D[7:0](BT.601), PCLK, HSYNC, VSYNC. So anyone who has reference design related that kindly give me.

*****STM32F407VET6

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
May 8, 2025

Hi @MURALISELVAM1992 

Video streaming over USB is feasible as the calculated throughput is within the capabilities of the USB HS interface. Here is an example.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

7 replies

Associate II
May 8, 2025

Thanks for sharing that but I need reference schematic like tested board's schematic. If you have kindly share me and Can we do video streaming via USB?

Andrew Neil
Super User
May 8, 2025

If it's not what you're looking for, why did you mark it as the solution?

To unmark it, see here.

 

You can't expect there to be an off-the-shelf design for every possible application just waiting for you;  at some point you are going to have to do some actual design work yourself - or pay someone to do it specifically for you...

 

Why do you particularly want to do this on an STM32F407VET6?

 

PS:

If you do want an off-the-shelf design, then just go by the performance/feature requirements you need - rather than the processor it runs on.

Sounds like a Raspberry Pi would do ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Peter BENSCH
ST Technical Moderator
May 8, 2025

[Unmarked the solution]

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
FBLBest answer
ST Technical Moderator
May 8, 2025

Hi @MURALISELVAM1992 

Video streaming over USB is feasible as the calculated throughput is within the capabilities of the USB HS interface. Here is an example.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL