2015-12-01 1:27 AM
Hello,
i try to generate Sourcecode for the Nucleo Board F303 RE with STM32 Cube. I Use the Toolchain MDK-ARM V5. At the code-generation I get the following message : The code is successfully generated under .... but MDK-ARM V5project generation have a problem. What may be the reason ? Best regards, Georg #keil-mdk-pro-stm32cube #stm32-cube2015-12-01 2:23 AM
Hi Georg,
1- If you are using an old version of CUBEMX, I recommend you to use the last version 2- Is it a recurrent issue or faced only one time?3- Maybe it is due to lack of space in your disk?4- Do you face the same issue with another machine?-Syrine –2015-12-01 6:55 AM
The error occurs
also with
the current
Version 4.11
.Previously I had
the older
version 4.10
installed
.
2 - The error occurs every time I try to generate code. 3 -The
space on the
hard disk is
not
too big, but
is
still
70GB
free
.
4 - Now I tried it on an other machine, and it works.The other machine
is
at least
a
workaround.
Thanks !We’re moving the ST Community to a new platform to give you a better and more reliable community experience.