2015-11-04 11:03 AM
Is there a tutorial/ resource page, where it I can find some guidelines about converting a KEIL project to IAR? I tried myself, but couldn't do it ( I am new in IAR toolchain). More specifically, I am looking to convert STM32L15XX_FLASH.ld and
startup_stm32l15XX_md_vl.s linker files into IAR compitable format. #iar #keil2015-11-04 12:17 PM
.ld suggests GNU linker script
There are IAR assembler files down in the CMSIS Device directoriesSTM32L1xx_StdPeriph_Lib_V1.3.1\Libraries\CMSIS\Device\ST\STM32L1xx\Source\Templates\iar\startup_stm32l1xx_md.sThe L1 Standard Peripheral Libraries come with a Template, clone the template, see that build and then add your own files. Use your merge tool of choice to bring things in.STM32L1xx_StdPeriph_Lib_V1.3.1\Project\STM32L1xx_StdPeriph_Templates\EWARM\Project.ewpDoing it from scratch, check the defines passed to the compiler, and manually add the files, and define the memory map of the part being used.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.