2025-01-27 6:41 AM
Hi,
I have a piece of CRC calculating code that I nicked from somewhere a couple of decades ago. I've been wondering about a few lines:
*CRCVal ^= (*CRCVal << 8) << 4;
*CRCVal ^= ((*CRCVal & 0xFF) << 4) << 1;(CRCVal is a pointer to a uint16_t variable.)
What I'm curious about is the slightly weird left-shifting notation. Shouldn't it give exactly the same result if it was written like this?
*CRCVal ^= (*CRCVal << 12);
*CRCVal ^= (*CRCVal & 0xFF) << 5;Does anyone have a hunch why the shifts are split up like this? Could it be something related to a specific compiler or device that handles half-byte shifts in a certain way?
By the way, it would be great if this forum had a "General programming" board. I prefer to ask questions here, as I think that the community has a nice vibe.
2025-01-28 12:39 AM
@EThom.3 wrote:Or perhaps an 8051, if that even had a C compiler 20-30 years ago. .
Keil C51 was well-established 20-30 years ago.
Keil was established as an 8051 tools company long before ARM bought them.
https://en.wikipedia.org/wiki/Keil_(company)
2025-01-28 12:44 AM
Interesting. Thanks.
Thus, my best guess is that the piece of code was originally made for either a PIC or an 8051.
2025-01-28 12:55 AM
Maybe by someone trying to write assembler in C: they didn't realise that the compiler can work out how to do a 12-bit shift - they didn't have to manually decompose it themselves?
Used to see a lot of that.
Also people thinking that cramming as much as possible into a single source line would produce less object code!
2025-03-27 3:12 AM
I just thought of something.
If this – quite old – code was indeed written for a PIC, it might have been written in an ancient MPLAB C compiler environment. Around the turn of the century, the MPLAB C17 compiler was not ANSI C compliant, had insane limitations, and was riddled with errors. If the CRC code was used in that environment, the doubled shifting operations might have been a work-around to get the code to compile correctly.
2025-03-27 4:19 AM
@Andrew Neil wrote:Also people thinking that cramming as much as possible into a single source line would produce less object code!
I have seen one guy removing whitespaces and empty lines, to make the program smaller. Or go faster – I'm not sure.
2025-03-28 7:36 AM
> I have seen one guy removing whitespaces and empty lines, to make the program smaller. Or go faster – I'm not sure.
Compressing whitespace in C does not affect program output.
2025-03-28 7:39 AM
Of course it doesn't. That's what made the guy's attempts mildly amusing.
2025-04-29 12:17 PM
Reminds me of some code I had:
int someMeaningfulName;
int describeTheContent;that was "improved" by someone to make it quicker to type the names:
int smn;
int dtc;This was in a place where they had no backups or version control, so there was no easy way back :(