Sending and receiving more then 4 bytes with SPI Block
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-10-27 11:49 PM
I'm working with MAT-TARGET for several months by now and it is a great tool.
In the past few days I encountered a problem regarding the maximum amount of bytes i can send throw the SPI Block (using Simulink R2019b) , while sending & receiving 4 bytes work well, when I try to increase the amount of bytes farther ( more then 4 bytes) I cannot uncheck the receive only box, meaning the SPI works only in receiving mode and cannot send data that is more then 32bits (4 Bytes in the SPI block configuration).
I was wondering if you can help me deal with that issue.
The SPI is configured to be full duplex master , 6.75Mb of baud rate, 8 bit data length.
Thanks in advanced!
Greg.
- Labels:
-
SPI
-
STM32-MatTarget