2024-09-16 6:35 AM - edited 2024-09-16 7:08 AM
I am encountering the FR_NOT_READY and FR_INVALID_OBJECT error when trying to mount the SD card and write a file in RVT101HVSFWCA0 Riverdi display. Could you please advise on how to resolve these issues?
2024-09-16 6:49 AM
Have you asked Riverdi ?
2024-09-16 7:06 AM - edited 2024-09-16 7:08 AM
Hello,
According to the examples provided under https://github.com/STMicroelectronics/STM32CubeH7/blob/master/Projects/STM32H745I-DISCO/Applications/FatFs/FatFs_Shared_Device/CM7/Src/main.c
I don't see that you linked the driver using FATFS_LinkDriver().
if(FATFS_LinkDriver(&MMC_Driver, MMCPath) == 0)
{
/* ..... Some code before */
FS_FileOperations();
}
}
static void FS_FileOperations(void)
{
FRESULT res;
uint32_t byteswritten, bytesread;
/* Register the file system object to the FatFs module */
if(f_mount(&MMCFatFs, (TCHAR const*)MMCPath, 0) != FR_OK)
{
goto error;
}
/* Some code after ... */
2024-09-16 8:36 AM
I reviewed the example you provided and corrected my code. The MX_FATFS_Init() function is executed before the StartCARDTask() function. Now I can mount the SD card but I still have the same error when using f_open() or f_write ().
2024-09-16 8:48 AM - edited 2024-09-16 9:02 AM
Hello,
Please use </> button to show your code instead of sharing a screenshots of it.
What errors you get for these APIs?
What if you use the same example (as it is) from what I posted and adapt it to your Hardware (clocks+IOs)? do you get the same behavior?
2024-09-16 9:02 AM
This is my code, I also tried your example and reconfigured the hardware but I still have the same error
uint8_t retSD; /* Return value for SD */
char SDPath[4]; /* SD logical drive path */
FATFS SDFatFS; /* File system object for SD logical drive */
FIL SDFile; /* File object for SD */
/* USER CODE BEGIN Variables */
/* USER CODE END Variables */
void MX_FATFS_Init(void)
{
/*## FatFS: Link the SD driver ###########################*/
retSD = FATFS_LinkDriver(&SD_Driver, SDPath);
/* USER CODE BEGIN Init */
StartCARDTask();
/* USER CODE END Init */
}
Disk_drvTypeDef disk = {{0},{0},{0},0};
/* Private function prototypes -----------------------------------------------*/
/* Private functions ---------------------------------------------------------*/
/**
* @brief Links a compatible diskio driver/lun id and increments the number of active
* linked drivers.
* @note The number of linked drivers (volumes) is up to 10 due to FatFs limits.
* @PAram drv: pointer to the disk IO Driver structure
* @PAram path: pointer to the logical drive path
* @PAram lun : only used for USB Key Disk to add multi-lun management
else the parameter must be equal to 0
* @retval Returns 0 in case of success, otherwise 1.
*/
uint8_t FATFS_LinkDriverEx(const Diskio_drvTypeDef *drv, char *path, uint8_t lun)
{
uint8_t ret = 1;
uint8_t DiskNum = 0;
if(disk.nbr < _VOLUMES)
{
disk.is_initialized[disk.nbr] = 0;
disk.drv[disk.nbr] = drv;
disk.lun[disk.nbr] = lun;
DiskNum = disk.nbr++;
path[0] = DiskNum + '0';
path[1] = ':';
path[2] = '/';
path[3] = 0;
ret = 0;
}
return ret;
}
/**
* @brief Links a compatible diskio driver and increments the number of active
* linked drivers.
* @note The number of linked drivers (volumes) is up to 10 due to FatFs limits
* @PAram drv: pointer to the disk IO Driver structure
* @PAram path: pointer to the logical drive path
* @retval Returns 0 in case of success, otherwise 1.
*/
uint8_t FATFS_LinkDriver(const Diskio_drvTypeDef *drv, char *path)
{
return FATFS_LinkDriverEx(drv, path, 0);
}
/**
* @brief Unlinks a diskio driver and decrements the number of active linked
* drivers.
* @PAram path: pointer to the logical drive path
* @PAram lun : not used
* @retval Returns 0 in case of success, otherwise 1.
*/
uint8_t FATFS_UnLinkDriverEx(char *path, uint8_t lun)
{
uint8_t DiskNum = 0;
uint8_t ret = 1;
if(disk.nbr >= 1)
{
DiskNum = path[0] - '0';
if(disk.drv[DiskNum] != 0)
{
disk.drv[DiskNum] = 0;
disk.lun[DiskNum] = 0;
disk.nbr--;
ret = 0;
}
}
return ret;
}
/**
* @brief Unlinks a diskio driver and decrements the number of active linked
* drivers.
* @PAram path: pointer to the logical drive path
* @retval Returns 0 in case of success, otherwise 1.
*/
uint8_t FATFS_UnLinkDriver(char *path)
{
return FATFS_UnLinkDriverEx(path, 0);
}
/**
* @brief Gets number of linked drivers to the FatFs module.
* @PAram None
* @retval Number of attached drivers.
*/
uint8_t FATFS_GetAttachedDriversNbr(void)
{
return disk.nbr;
}
void StartCARDTask(void)
{
for (;;)
{
MX_SDMMC1_SD_Init();
HAL_SD_MspInit(&hsd1);
HAL_SD_MspDeInit(&hsd1);
osDelay (1);
// Montar el sistema de archivos
res = f_mount(&SDFatFS, (TCHAR const*)SDPath, 0);
if (res == FR_OK)
{
printf("Tarjeta SD montada correctamente en la unidad '0:'.\n");
res = f_open(&SDFile, "prueba", FA_CREATE_ALWAYS | FA_WRITE);
if (res == FR_OK)
{
// Escribir datos en el archivo
res = f_write(&SDFile, "Hola, Mundo!", 12, &bw);
if (res == FR_OK && bw == 12)
{
printf("Archivo creado y escrito correctamente.\n");
}
else
{
printf("Error al escribir en el archivo.\n");
}
f_close(&SDFile);
}
else
{
printf("Error al abrir el archivo.\n");
}
}
else
{
printf("Error al montar la tarjeta SD. Código: %d\n", res);
}
f_mount(NULL, "", 1);
// Terminar la tarea
osThreadTerminate(NULL);
}
osDelay (10000) ;
}
2024-09-16 9:04 AM - edited 2024-09-16 9:05 AM
If you tried the example as it is and didn't work, you need to check your SD card: it could be corrupted or not compatible.
2024-09-16 9:18 AM
I am using a type 10 SD card (10MB/s), which one do you recommend?
2025-06-06 12:45 PM
res = f_mount(&SDFatFS, (TCHAR const*)SDPath, 0);This means that the SD card is not mounted immediately.
FRESULT f_mount (
FATFS* fs, /* Pointer to the filesystem object to be registered (NULL:unmount)*/
const TCHAR* path, /* Logical drive number to be mounted/unmounted */
BYTE opt /* Mount option: 0=Do not mount (delayed mount), 1=Mount immediately */
)