2019-04-24 4:47 AM
I'm using the STM32 MAT plugin and embedded coder for Simulink to generate C-Code out of my models to compile them onto an STM32F4. As IDE I use TrueStudio and for my MCU Configuration I use CubeMX.
Because my discrete solver step time in Simulink is set, it seems that the embedded coder tries to make a Software based Interrupt every 0.001 seconds.
#include "main.h"
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
#include
#include "untitled.h" /* Model's header file /
#include "rtwtypes.h" / MathWorks types */
extern RT_MODEL_untitled const untitled_M;
extern void untitled_SetEventsForThisBaseStep(boolean_T);
static boolean_T OverrunFlags[1];
static volatile uint32_t autoReloadTimerLoopVal_S = 1;
static volatile uint32_t remainAutoReloadTimerLoopVal_S = 1;
int main(void)
{
int_T i;
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
/* Systick configuration and enable SysTickHandler interrupt */
if (SysTick_Config((uint32_t)(SystemCoreClock * 0.001))) {
autoReloadTimerLoopVal_S = 1;
do {
autoReloadTimerLoopVal_S++;
} while ((uint32_t)(SystemCoreClock * 0.001)/autoReloadTimerLoopVal_S >
SysTick_LOAD_RELOAD_Msk);
SysTick_Config((uint32_t)(SystemCoreClock * 0.001)/autoReloadTimerLoopVal_S);
}
remainAutoReloadTimerLoopVal_S = autoReloadTimerLoopVal_S;//Set nb of loop to do
for (i=0;i<1;i++) {
OverrunFlags[i] = 0;
}
untitled_initialize();
while (1) {
/*Process tasks every solver time*/
if (remainAutoReloadTimerLoopVal_S == 0) {
remainAutoReloadTimerLoopVal_S = autoReloadTimerLoopVal_S;
/* Check base rate for overrun */
if (OverrunFlags[0]) {
rtmSetErrorStatus(untitled_M, "Overrun");
}
OverrunFlags[0] = true;
/* Step the model for base rate */
untitled_step();
OverrunFlags[0] = false;
}
}
}
/* SysTick_Handler callback function*/
/*This handler is called every tick and schedules tasks*/
void HAL_SYSTICK_Callback(void)
{
/* For TIME OUT processing */
HAL_IncTick();
/* Manage nb of loop before interrupt has to be processed */
if (remainAutoReloadTimerLoopVal_S) {
remainAutoReloadTimerLoopVal_S--;
}
}Unfortunately when I try to run the Code, nothing happens. The Compiler always stucks at the if condition in the while (1) Loop. So I see that there's something wrong here with the Interrupt handling, but I don't know how to resolve the issue. Probably you can help
2019-08-20 3:28 AM
Hi @Tstro.12 ,
The version 5.1.0 of STM32-MAT/TARGET has just been released at the end of July 2019.
Be aware that a lot of changes were involved in this release with respect to the timer (in detail, alignment with STM32CubeMX version 5.1.0).
It is strongly recommended to upgrade to the most recent version of STM32-MAT/TARGET.
Regards.
Cyril