2019-02-26 11:54 PM
I have tried using the examples to generate the code , but it seems it does not create an MDK-ARM project. I only see the Matlab generated files but no MDK-ARM project which I can flash directly to the device.
I was previously using Matlab 2015b, Windows 7, STM32 embedded target for MATLAB® and Simulink® release 4.1.1 and Cube Mx 4.7.1 and I have no problem generating the code from Matlab. Not quite sure if it is the Windows 10 causing the problem or something else.
Thanks!
2019-08-20 3:31 AM
Hi @jessica ,
The version 5.1.0 of STM32-MAT/TARGET has just been released at the end of July 2019.
Be aware that a lot of changes were involved in this release (in detail, alignment with STM32CubeMX version 5.1.0).
It is strongly recommended to upgrade to the most recent version of STM32-MAT/TARGET.
Regards.
Cyril
2019-09-02 8:37 PM
Hello @Cyril FENARD
Thanks for the heads up. Would you know if the G4 device is already supported in the latest version of the STM32-MAT/TARGET?
Regards,
Jessica
2019-09-03 1:12 AM
Hi @jessica ,
G4 devices must use the recent STM32CubeMX tool after 5.1.0 version.
With the release of STM32-MAT/TARGET at the end of July 2019, you are able to start using G4 in your Simulink model (Prepare/update configuration and tool path for STM32CubeMX 5.3.0 for instance).
An official version by the end of 2019 is planned for STM32-MAT/TARGET, which will demonstrate use-cases with G4.
Regards.
Cyril