cancel
Showing results for 
Search instead for 
Did you mean: 

FreeRTOS and BSP Drivers ST32L152D-EvalBoard STM32CubeL1

anio1491
Associate II
Posted on April 22, 2016 at 15:02

Hello,

I want to integrate the FreeRTOS and the BSP drivers in the same project for the ST32L152D-EvalBoard. I am doing my project in Atollic TrueSTUDIO and I am using the code from STM32CubeL1.

Is there an easy way to do that: should I start with the FreeRTOS application and add the drivers on top, or should I start with e.g. the LCD example, and then include the FreeRTOS files?

Thank you! Any idea would help me!

#hal #atollic #bsp #freertos
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0