2021-11-23 1:32 AM
In the example projects there is no dedicated __ARMCC_VERSION (ARM compiler V6).
file: stm32_wpan_common.h, in the BleHeartRateRTOS example
#if defined ( __CC_ARM )
#if defined (__ARMCC_VERSION) && (__ARMCC_VERSION >= 6010050U) //We never get here! jumping to gcc
#define PACKED__ __attribute__((packed))
#define PACKED_STRUCT struct PACKED__
#else
#define PACKED__(TYPE) __packed TYPE
#define PACKED_STRUCT PACKED__(struct)
#endif
#elif defined ( __GNUC__ )
#define PACKED__ __attribute__((packed))
#define PACKED_STRUCT struct PACKED__
#elif defined (__ICCARM__)
#define PACKED_STRUCT __packed struct
#else
#define PACKED_STRUCT __packed struct
#endifBest case, it is hiding under __CC_ARM (ARM compiler V4/5), sometimes like in the PLACE_IN_SECTION it is not even under a define.
There are differences between compilers regarding the __attribute__ keyword as specified in :
https://www.keil.com/support/man/docs/armclang_mig/armclang_mig_chr1398848377314.htm
issue:
1. The code is forcing me to use gcc (__GNUC__) when I have __ARMCC_VERSION (ARM compiler V6).
2.How do I translate it to the __ARMCC_VERSION (ARM compiler V6) ?
3.PLACE_IN_SECTION does not work in __ARMCC_VERSION (ARM compiler V6) , gives different final addresses to variables.
PLACE_IN_SECTION("MB_MEM1") ALIGN(4) static TL_CmdPacket_t BleCmdBuffer;Why is that?