Others: STM32 MCUs related

Find out more about STM32 implementations with external components, discuss use cases, and discover how to use new tools and ST components.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32f429bit6 LTDC Background Problem

having trouble with the background displaying center on the adafruit 5 inch LCD CH500WV05A-T wondering if anyone has used this lcd with stm32f4 and have the HSW HBP HFP VSW VBP VFP values you used  im guessing this is the issue ive used the ones from...

BMP581 data problem

bmp581 data problemI'm using a BMP581 barometric pressure sensor on my custom flight computer designed for a rocket project. The altitude data I read from the sensor is not stable over time. While the sensor is in a stationary position (not moving), ...

AT24CM02-SSHD I2C ERROR

I use STM32F767NIH6.I save data to AT24CM02-SSHD with I2C.However, I divide it into several areas and save the necessary data.For example, I save data such as setting values, measurement values, etc. separately.However, when saving data in some areas...

Seyoung by Associate II
  • 349 Views
  • 3 replies
  • 1 kudos

UART reception error

Hello,I am using Nucleo f446re board to interface with a sensor over UART. sensor is able to send the response data frame  over rx line to mcu as mcu sends uart frame.This transaction or data transfer is visually verified using logic analyser.Actual ...

Resolved! Keil debugger initiliazation file for STM32H753

Hello everyone,I need a starting INI file for an STM32H753.I'm using the NUCLEO-H753ZI evaluation board.I'm using sample projects for various peripherals: GPIO, ADC, TIM, ... . My IDE is Keil uVision.Using the sample projects, it's easy to debug the ...

Ma2teo by Associate
  • 392 Views
  • 1 replies
  • 0 kudos