Skip to main content
NitishGhadage
Associate
November 13, 2024
Solved

XBEE XR868 with stm32l431rct6 controller problem

  • November 13, 2024
  • 4 replies
  • 1439 views

Hey, I am working on Xbee with stm32, and I am getting a big problem while connection. 


I am using two Xbee's one is configured as a standard router which is connected to UART1 of the 
stm32 controller and the other is configured as a coordinator which is connected to the com port of another system through RS485 cable to XCTU. I have to use them in API mode. I have configured both of them in API Mode, now I am able to send API data frame from router to coordinator , but I cant receive API frame from coordinator to router ? 

When I send a simple API frame from the coordinator to the router, the router Xbee sends an acknowledgment frame back to the coordinator, but my controller does not receive any frame, I have written the code to receive the complete frame at once using the polling method as well as interrupt method as well as to fetch the data in single-byte also. But it's not working. Data is received up to Xbee but the controller does not receive anything. It stops the further processing. 

Screenshot (21).png

See first router sends some random message to coordinator, then from coordinator I have sent Sample data frame to router , it acknowledges back but after that router should send received data back to coordinator , but its not processing? 

 

This topic has been closed for replies.
Best answer by NitishGhadage

Got the solution. It's not the problem of STM. It was related to the XBEE module built-in protocol. It's like, when you power on XBee and if it is in API mode, it sends the MODEM STATUS frame to uart of 6 bytes. And that's why the problem persists. So inside the stm program, you have to first receive these 6 Bytes ofthe  frame and then start UART functioning and UART interrupts. It will work perfectly.

4 replies

Visitor II
November 27, 2024

I am experiencing a similar issue with my setup. I have one XBee module connected to an STM32 microcontroller via UART and another XBee connected to my PC through RS485. The module on the PCB (connected to the STM32) successfully sends data, but it does not receive any frames from the module connected to the PC. I am looking for a solution as well. Have you been able to resolve this issue?"

 

Andrew Neil
Super User
November 27, 2024

The only thing here specific to the STM32 is your UART handling.

How have you confirmed that 

  1. The XBee is receiving correct commands from the STM32;
  2. The STM32 is correctly receiving responses from the XBee.

If that's all correct, then it's an XBee issue - nothing to do with ST - so you need to go to Digi for support with that:

https://www.digi.com/support

https://forums.digi.com/

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
NitishGhadage
NitishGhadageAuthorBest answer
Associate
February 11, 2025

Got the solution. It's not the problem of STM. It was related to the XBEE module built-in protocol. It's like, when you power on XBee and if it is in API mode, it sends the MODEM STATUS frame to uart of 6 bytes. And that's why the problem persists. So inside the stm program, you have to first receive these 6 Bytes ofthe  frame and then start UART functioning and UART interrupts. It will work perfectly.

mƎALLEm
ST Technical Moderator
November 27, 2024

Thread moved to Others: hardware and software. If an UART issue is confirmed, it will be moved back to STM32 MCU product forum board.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.