cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong option byte using Rflasher and ST visual programmer

remi23
Associate II
Posted on August 18, 2010 at 15:27

Hi all

I just wanted to flag a problem with the Rflasher and ST visual programmer  regarding the chip ST72F521M9

Ride7:                          7.30.10.0159

Rkit STM8 for ride 7      2.30.10.075

Ride 7 patch                 7.30.10.169

=> The option byte calculated via those software are WRONG!

I figured out that by entering manually the hexadecimal option byte everything works eg:''27 87''

Hopefully this will be taken into account for the next release of the software...

Thanks for your time

Best regards

Rémi

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
LaurentL
ST Employee
Posted on September 03, 2010 at 10:48

Hi,

For Rflasher soft, it's Raisonance.

Which version of STVP ?

Download and install the latest, you have to choose ST72F521x9 on STVP and TQFP80 is the default package.

The error is on which bit(s)?

On Package bits?

Rgds,

Laurent