cancel
Showing results for 
Search instead for 
Did you mean: 

workaround for the STR9 errata 2.5

daves
Associate
Posted on October 21, 2009 at 19:44

workaround for the STR9 errata 2.5

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
daves
Associate
Posted on May 17, 2011 at 09:59

I'm implementing the workaround for the STR9 errata 2.5 ''Flash frequency limitation when programming'' and discovered that the EMI_BCLK might be affected when I change the FMICLK frequency. I'm using the BCLK to drive a PLL in an FPGA and the PLL is losing lock temporarily.

I suspect that writing to the SCU_CLKCNTR register is affecting the other clocks. Is this true? Is there another workaround I can use?

-Dave