cancel
Showing results for 
Search instead for 
Did you mean: 

What is the real current accuracy in VND5025? DS says K1 is 2810 +/- something equal to about 30-35%. Is that steady and can therefore be calibrated away? The current sense ratio drift for K1 is +/- 10%. Should i then add these two if I not calibrate?

Henrik1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @Henrik​, to the community!

Well, the factors K0, K1... are based on a current derived from the load current, which, however, does not have a high-precision reference voltage like an ADC. For this reason, the K factors have a relatively large tolerance and also non-negligible drift. Incidentally, the drift is not to be added to the error of the K-factors, but multiplied.

However, there is the possibility to calibrate the K-factor, which is shown in detail in UM1556, section 2.7.3.

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @Henrik​, to the community!

Well, the factors K0, K1... are based on a current derived from the load current, which, however, does not have a high-precision reference voltage like an ADC. For this reason, the K factors have a relatively large tolerance and also non-negligible drift. Incidentally, the drift is not to be added to the error of the K-factors, but multiplied.

However, there is the possibility to calibrate the K-factor, which is shown in detail in UM1556, section 2.7.3.

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.