2005-02-03 4:16 AM
2005-01-27 9:16 PM
Hi
what do i need to imlement an TCP/IP stack with STR710? I am looking at porting of uCLinux with TCP/IP functionality and the STE10/100 device. I would like to know if are there different way and more easy respect this. Tks2005-01-28 12:35 AM
Hi dimarcog,
I'am very interested by your application, Could You please inform us what kind of design or development of TCP/IP on STR710 ? How will you connect STE10/100 ? If you Need 10Mbits or 100Mbits baud rate ?.... But It seems to me that STE10/100 is a bit complex to connect to STR710 as it has a PCI bus interface ! With Regards, :-] [ This message was edited by: Rave on 28-01-2005 14:06 ] [ This message was edited by: Rave on 28-01-2005 14:07 ]2005-01-31 5:35 AM
Hi,
I guess there are very very interest around the TCP/IP implementation on STR7. I hope the moderators give us the information needed or other information in order to use STE or a different devices or solution.2005-01-31 11:32 PM
Hi,
I've just got my hardware (own design, not eval board) and is starting currently it up. We (the company I work for) have choosen the Davicom DM9000 as ethernet controller. It has a standard ISA bus which is very easy to interface to the ARM. I'm planning to use the lwIP TCP/IP stack which is an open source solution. http://savannah.nongnu.org/projects/lwip/ Regards /Beach/2005-02-02 6:25 AM
Hi Beach,
the DM9000 is very interest. Regarding IwIP TCP/IP stack you have to make the porting for ARM. May be to easy to use a uCLinux porting in order to reuse the Linux driver for DM9000, am I right?2005-02-03 1:37 AM
Hi.
I think uCLinux is the best option, not just for reuse, but for what you can do after you have uCLinux running (gcc, tcp/ip stack, file system, etc). Hernán Sánchez2005-02-03 2:02 AM
Hi,
RealTek RTL8019 and Cypress CY8900 Ethernet Controller seem also very simple to connect with STR710 EMI Interface (16-bits), kind regards, :p2005-02-03 4:16 AM
Hi,
Just for clarification. I'm planning to use the lwIP TCP/IP stack and not uCLinux because I only want/need the TCP/IP stack. I dont need all the other OS stuff in the current project. Maybe I will have a look at the 'low_level' stuff in the DM9000 driver for the uCLinux to see how to initialize the chip. /Beach