cancel
Showing results for 
Search instead for 
Did you mean: 

CAD files for STR710 and STR720 Eval Boards

richardrooney
Associate II
Posted on February 04, 2005 at 12:05

CAD files for STR710 and STR720 Eval Boards

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
richardrooney
Associate II
Posted on January 28, 2005 at 23:15

Can someone please supply me with CAD source files for the STR710 and STR720 Eval Boards ? (I presume they were developed using Orcad - most eval boards are ...)

hichem2
Associate II
Posted on January 31, 2005 at 09:18

Hello cadrjr,

Please can you explain ,what does means ''CAD source files ''

it is a matter of ''gerber'' file or not ?

With regards.

Hich :-]

richardrooney
Associate II
Posted on January 31, 2005 at 13:33

I principly mean the Schematics in Electronic format (ORCAD, etc). (I have them in .pdf format already.)

Also any Layout files would be useful - files containing the device footprints would save me having to re-enter them all again.

Gerber files are of no use.

(The files I need are *.opj, *.dsn , *.olb and *.max if Orcad was used)

Thanks

:)

hichem2
Associate II
Posted on February 01, 2005 at 12:09

Hello cadrjr,

Our design engineer use the Mentor tool to develop the Electronic Schematics and Gerber file is the only file we've got.

Hope that helps.

Best regards,

Hich. :p

hichem2
Associate II
Posted on February 03, 2005 at 04:36

Hello cadrjr

You find attached the mentor files attached with this message.

Hope that helps!

Cheers

Hich :p

________________

Attachments :

mb393a.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Ht9a&d=%2Fa%2F0X0000000aJh%2F4j_WtyhOPzM2d2Hkj7Wqv3Xp6aGgNt78TQmXdkXN6d8&asPdf=false
richardrooney
Associate II
Posted on February 04, 2005 at 12:05

Thanks - but these are only Gerber filers for PCB manufacture.