cancel
Showing results for 
Search instead for 
Did you mean: 

stwlc98 TX mode

Hisanori
Associate

What steps are required to set stwlc98 to TX mode?

If you set 0x0020 to 01, 0x000E becomes 03.

However, AC1 and AC2 do not cause burst oscillation.

The Optional (TX mode only) circuit is on the board, and VOUT is connected to 5V.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
wei
Associate

I have the same question, I connected VOUT to 12V in my project.

The receiver was verified with other solution.

Hoping someone can answer this.

Hisanori
Associate

This issue is still unresolved.Please tell me the solution.

simonh
Associate III

Hello,

Is there alreadya solution for this problem? Is there any application note or some other more detailed description for the TX mode?

 

My problem is the following:

I want to transmit 15W, but the STWBC86 can only transmit 5W. So I have to deal with the STWBC2-HP, but this one is too big for my application and has too much functionality I do not need.

 

Thank you
Simon

willzhou
ST Employee

STWLC98 support TX mode, please check this link at page 44 5.15 Transmitter (Tx) mode

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you, but do you have more Information how I can set up the software correctly, to get the TX mode working?