cancel
Showing results for 
Search instead for 
Did you mean: 

STVD works fine with windows 7; W10 64bit I failed to install

RobK1
Senior II

Split from Is STM8 recomended for beginners?

Originally in reply to this post.


STVD Version 4.3.12 (August 4, 2017!!) runs fine here on W11.

3 REPLIES 3
DarekR
Associate III
In 2021 I tried to install STVD on W10-64bit and failed. On the other hand, I have Ubuntu Linux next to windows and I installed W7 and STVD on virtualbox there. I didn't try to install it on windows later.

I guess that VirtualBox is the cause of the problem. I've tried to use STVD on VirtualBox with Windows XP SPII and Cosmic did not request a license as it was on Windows 11 (without VirtualBox).

In Windows 10 I installed without virtualbox.