cancel
Showing results for 
Search instead for 
Did you mean: 

STR755FR2 has a start-up problem?

y_25
Associate II
Posted on August 17, 2008 at 04:13

STR755FR2 has a start-up problem?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
y_25
Associate II
Posted on August 16, 2008 at 12:20

Hi, all.

I'm using STR755FR2 in my project(system 5vcc). For debug purpose, I loaded a simple program that toggles the LED using tim0 in 200ms. When I power on, it sometimes runs and sometimes not. Firstly I thought the problem was about Reset Supervisor and I tried several Reset Supervisors including STM1813 which ST reccomends, but nothing changed. The same behaviour also occurs at Watchdog reset.

Do you have any information about STR755FR2 has a start-up problem or what can be the problem?

y_25
Associate II
Posted on August 17, 2008 at 04:13

now,this is ok!