2025-12-14 5:30 AM - last edited on 2025-12-14 8:10 AM by mƎALLEm
i am using bluepill board. which PA9,PA10 is connected to header. when i connect FTDI as RX Tx mode and also i cheked REST status(reset is high if switch not pressed) but cube programmer say exact like you. my target chip is STM32F103C8T6. using clone stlink i found chip id is 0x414 and flash memory is 256Kb which is not according to datasheet of that MCU.
2025-12-14 8:09 AM - edited 2025-12-14 8:11 AM
Hello,
Clone STLINKs and Blue Pills boards are not ST products. Blue Pill boards contain conterfeit chips.
2025-12-14 11:16 AM - edited 2025-12-14 12:02 PM
Your chip might be genuine STM , just a bigger one:
Try using it as F103C8 , or try start a project for F103CC and generate code and try debug with a simple test program.
Then you know: chip working fine - or not.
Probably its just this way: today its more expensive to produce six different dies/chips , just because of different flash/ram size, than just one "big" and still can sell it at all sizes , or even better: the "bad" chips, memory not working at full size, still no waste, can sell it at the smaller size type and save money.
And you could be lucky: got a F103 with 256K flash at the price of 64K chip. :)
(or its a fake - just test it.)
die 414 could be:
die 410:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.