cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 USB Host HS not detecting USB

embedded-jsd
Visitor

I have connected and an external HS PHY to STM32F427VGT6 through ULPI pins.
Configured USB_OTG_HS in Host Only mode for external Phy with parameter Settings as

Speed: High Speed 480MBits/s 
Enable internal IP DMA: Disabled
Physical Interface: External Phy
Use External VBUS: Enabled
Signal Start of Frame: Disabled

In NVIC settings for USB_OTG_HS all three available interrupts are enabled. 

USB On The Go HS End Point 1 Out global interrupttrue00
USB On The Go HS End Point 1 In global interrupttrue00
USB On The Go HS global interrupttrue00


In Middleware Packages USB_ Host, FATFS is configured according to attached image.
MCU schematic and USB-PHY schematic is also attached.

The problem i am facing is STM32 is not detecting USB and gstate of USB always remain to HOST_IDLE, even if i connect or disconnect pendrive.

1 REPLY 1
FBL
ST Employee

Hello @embedded-jsd 

Do you reproduce using a reference board?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL