cancel
Showing results for 
Search instead for 
Did you mean: 

ST7 problem

pete3
Associate II
Posted on September 16, 2005 at 07:07

ST7 problem

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
pete3
Associate II
Posted on September 15, 2005 at 10:49

Hi all,

I have narrowed a code error down to this loop:

while(!(CMSR & 0x01))

{

CMCR |= 0x01;

}

from which the COSMIC compiler generates the following absolute listing:

1235 850d 2002 jra L572

1236 850f L372:

1237 ; 444 CMCR |= 0x01;

1238 850f 1068 bset _CMCR,#0

1239 8511 L572:

1240 ; 441 while(!(CMSR & 0x01))

1241 8511 0169fb btjf _CMSR,#0,L372

The problem is that the code is entered and runs either once or twice (normally twice, ~70% chance) but then code execution stops! I have checked this using SCI comms code and code immediately after this loop will not run. Code before this runs as expected.

Does anyone have any ideas? I am programming the micro through an inDART ST7 which works fine.

alok2
Associate II
Posted on September 16, 2005 at 04:25

What is the purpose of this code ? CMSR is a register ? Why loop is running 2 times , it shall be always once

change it to

if (!(CMSR & 0x01))

{

CMCR |= 0x01;

}

pete3
Associate II
Posted on September 16, 2005 at 07:07

Sorry alok,

CMSR is a status register. To put the CAN peripheral into initialisation mode, you need to set bit 0 of the CMCR register. It will then enter that mode when it is not receiving anything. I cannot guarantee that the module is doing nothing when this code runs, but the next lines require that the CAN module is in initialisation. When bit 0 of the CMSR is set, the module is in initialisation mode.

My problem is that this code executes fine but that the line directly after it never executes.