cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F276 XFLASH access timing questions

tom7
Associate II
Posted on October 27, 2004 at 07:13

ST10F276 XFLASH access timing questions

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
tom7
Associate II
Posted on October 26, 2004 at 13:32

My customers ST10F276 hardware runs on 48 Mhz.

Does someone know how to setup the required 1 wait-state for the XFLASH ?

Does someone know the program execution speed difference between IFLASH and XFLASH ?

thx, tomas.

charles239955_st
Associate II
Posted on October 26, 2004 at 14:13

Hello,

The 1 wait-state for the XFlash must be configured by writing to the XFICR register at address 0x0E'E000. The reset value in 0x000F which is configuring the XFlash access with 15 wait states.

To have 1 wait-stae the value 1 must be written into.

If the register is not defined in your toolchain you can define it as follow:

#define XFICR *(_huge unsigned int *)(0x000EE000)

for Tasking toolchain

#define XFICR *( unsigned int huge *)(0x000EE000)

for Keil toolchain

Concerning the execution speed, if we do not take into account the wait state, then the execution speed is already not equivalent between IFlash and XFlash.

The IFlash is connected through a 32bit data bus while the XFlash is connected through a 16bit data bus.

Some of the ST10 instructions are coded on 32bit (as JMPS, CALLS...).

For these instructions, each fetch on the IFlash which provide the entire opcode.

But when executing from XFlash 2 accesses will be necessary to provide the full 32bit instruction to the CPU.

It is difficult to give a ratio of speed exceution between IFlash and XFlash as it will depend a lot of the code (number of 32bit vs 16bit instructions).

At 48MHz it will give:

- 41,6ns of instruction cycle from IFlash

- 62.5 ns from XFlash, 1 wait state, 16bit instruction

- 135 ns from XFlash, 1 wait state, 32bit instruction

Hope this is clear.

Kenshin

tom7
Associate II
Posted on October 27, 2004 at 07:13

thx kenshin.