cancel
Showing results for 
Search instead for 
Did you mean: 

SSP1 interrupt Problem

lillian_200601
Associate II
Posted on December 20, 2007 at 14:09

SSP1 interrupt Problem

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
lillian_200601
Associate II
Posted on May 17, 2011 at 11:32

Hi Everybody,

I am quite new to STR912 and please allow me to ask the simple questions.

I am using MTBSTR9 eval board and Keil MDK to implement SPI communications.

SSP0 sends data out as the master device and SSP1 receives data as the slave.

Enable SSP1_IT_RxFifo interrupt in order to receive data from SSP0.

The issue is that I get only one time SSP1_IT_RxFifo interrupt and then cannot get in the interrupt any more. Could you please take a look at my code and give me a clue what I may miss?

Many many thanks.

The following is my code for SSP0 and SSP1 configuration.

/* SCU configuration */

SCU_Configuration();

/* GPIO pins configuration */

GPIO_Configuration();

SSP_DeInit(SSP0);

SSP_InitStructure.SSP_FrameFormat = SSP_FrameFormat_Motorola;

SSP_InitStructure.SSP_Mode = SSP_Mode_Master;

SSP_InitStructure.SSP_CPOL = SSP_CPOL_High;

SSP_InitStructure.SSP_CPHA = SSP_CPHA_2Edge;

SSP_InitStructure.SSP_DataSize = SSP_DataSize_8b;

SSP_InitStructure.SSP_ClockRate = 5;

SSP_InitStructure.SSP_ClockPrescaler = 2;

SSP_Init(SSP0, &SSP_InitStructure);

/* SSP1 configuration */

SSP_DeInit(SSP1);

SSP_InitStructure.SSP_Mode = SSP_Mode_Slave;

SSP_InitStructure.SSP_SlaveOutput = SSP_SlaveOutput_Enable;

SSP_Init(SSP1, &SSP_InitStructure);

/* Enable SSP1 receive interrupt */

SSP_ITConfig(SSP1, SSP_IT_RxFifo|SSP_IT_RxTimeOut, ENABLE);

// SSP1 interrupt configuration

// VIC0 configuration

VIC_DeInit();

VIC_Config(SSP1_ITLine, VIC_IRQ, 1);

VIC_ITCmd(SSP1_ITLine, ENABLE);

/* SSP0 enable */

SSP_Cmd(SSP0, ENABLE);

/* SSP1 enable */

SSP_Cmd(SSP1, ENABLE);

while(Tx_Idx

{

SSP_SendData(SSP0, SSP0_Buffer_Tx[Tx_Idx++]);

}

*******************

SSP1 receive inerrupt route:

void SSP1_IRQHandler(void)

{

while(SSP_GetFlagStatus(SSP1, SSP_FLAG_RxFifoNotEmpty)==SET)

{

SSP1_Buffer_Rx[Rx_Idx++] = SSP_ReceiveData(SSP1);

}

SSP_ClearFlag(SSP1, SSP_FLAG_RxFifoNotEmpty);

VIC0 ->VAR = 0;

VIC1 ->VAR = 0;

}