cancel
Showing results for 
Search instead for 
Did you mean: 

Setting PWM Output

daryl2
Associate II
Posted on March 09, 2008 at 23:44

Setting PWM Output

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
daryl2
Associate II
Posted on March 07, 2008 at 06:54

Hi,

I am trying to generate PWM output using the STR750 MCU. Below are my settings. Somehow I am not able to get any PWM signals out. Anyone has any idea why this is so? Please enlighten me. Thank you very much

// PWM, TIM0, TIM1 and TIM2 clock has been enabled

PWM_InitTypeDef PWM_InitStructure;

/* Configure P1.06 as alternate function (PWM_OC2) */

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

GPIO_Init(GPIO1, &GPIO_InitStructure);

// PWM configuration

PWM_InitStructure.PWM_Mode = PWM_Mode_PWM;

PWM_InitStructure.PWM_Prescaler = 0x00; // TIM_CLK: 60 MHz

PWM_InitStructure.PWM_CounterMode = PWM_CounterMode_Up;

PWM_InitStructure.PWM_Period = 0x7530; // PWM frequency : ~2KHz

PWM_InitStructure.PWM_Channel = PWM_Channel_2;

PWM_InitStructure.PWM_Pulse2 = 0x3A98; // Duty cycle: 50%

PWM_InitStructure.PWM_Polarity2 = PWM_Polarity2_Low;

PWM_InitStructure.PWM_Polarity2N = PWM_Polarity2_Low;

PWM_InitStructure.PWM_Complementary = PWM_Complementary_Disable;

PWM_InitStructure.PWM_OCState = PWM_OCState_Disable;

PWM_InitStructure.PWM_OCNState = PWM_OCNState_Enable;

PWM_InitStructure.PWM_DeadTime = 0;

PWM_Init(&PWM_InitStructure);

PWM_Cmd(ENABLE);

jpeacock2
Associate II
Posted on March 07, 2008 at 13:03

Do you have the PWM peripheral clock enabled?

MRCC_PeripheralClockConfig(MRCC_Peripheral_PWM, ENABLE);

This is how I use the PWM channels:

Code:

/* PWM is configured to generate a 3Khz pulse with CK_TIM = 60MHz:

* update frequency = CK_TIM/(Prescaler+1)(Period+1) = 300 Hz

* The blower motor(s) require a PWM signal with a frequency of 150hz to 400hz.

* A 100% duty cycle is on full, while a 0% duty cycle is completely off.

*/

PWM_DeInit(); /* reset PWM */

/* Configure blowers as PWM* outputs */

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_6 | GPIO_Pin_8;

GPIO_Init(GPIO1, &GPIO_InitStructure); /* blower motors */

MRCC_PeripheralClockConfig(MRCC_Peripheral_PWM, ENABLE); /* PWM clock source enable */

/* PWM Channel 1 configuration: main ball blower */

PWM_InitStructure.PWM_Mode = PWM_Mode_PWM;

PWM_InitStructure.PWM_Prescaler = 19999; // prescale by 60Mhz/20000 = 3Khz

PWM_InitStructure.PWM_CounterMode = PWM_CounterMode_Up;

PWM_InitStructure.PWM_Period = BLO_OFF - 1; // divide 3Khz /10 = 300Hz

PWM_InitStructure.PWM_Complementary = PWM_Complementary_Enable; // enable inverted output pins

PWM_InitStructure.PWM_Channel = PWM_Channel_1;

PWM_InitStructure.PWM_Pulse1 = BLO_OFF; // startup motor off

PWM_InitStructure.PWM_DTRAccess = PWM_DTRAccess_Disable;

PWM_InitStructure.PWM_Polarity1N = PWM_Polarity1N_Low; // PWM1N active lo (invert to FET)

PWM_InitStructure.PWM_RepetitionCounter = 0x05;

PWM_Init(&PWM_InitStructure);

/* PWM Channel 2 configuration: eject ball blower */

PWM_InitStructure.PWM_Channel = PWM_Channel_2;

PWM_InitStructure.PWM_Pulse2 = BLO_OFF; // startup motor off

PWM_InitStructure.PWM_Polarity2N = PWM_Polarity2N_Low; // PWM2N active lo

PWM_Init(&PWM_InitStructure);

/* PWM Channel 3 configuration: unused */

PWM_InitStructure.PWM_Channel = PWM_Channel_3;

PWM_InitStructure.PWM_Pulse3 = BLO_OFF; // startup motor off

PWM_InitStructure.PWM_Polarity3N = PWM_Polarity3N_Low; // PWM3N active lo

// no dead time, no emergency stop

PWM_InitStructure.PWM_DTRAccess = PWM_DTRAccess_Enable;

PWM_InitStructure.PWM_Emergency = PWM_Emergency_Disable;

PWM_InitStructure.PWM_DeadTime = 0x00;

PWM_InitStructure.PWM_LOCKLevel = PWM_LOCKLevel_3;

PWM_InitStructure.PWM_OSSIState = PWM_OSSIState_Enable;

PWM_Init(&PWM_InitStructure);

/* Enable PWM Main Outputs */

PWM_CtrlPWMOutputs(ENABLE);

/* Enable PWM counter */

PWM_Cmd(ENABLE);

To set the duty cycle takes one line:

PWM_SetPulse(PWM_Channel_1, value0to99);

daryl2
Associate II
Posted on March 09, 2008 at 23:44

thanks jakbird. Managed to solve my problem. My code did not run PWM_CtrlPWMOutputs(ENABLE).