cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding JTAG Testing ....... Urgent

sharusid
Associate II
Posted on May 20, 2005 at 13:13

Regarding JTAG Testing ....... Urgent

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
sharusid
Associate II
Posted on May 17, 2011 at 12:07

Hello

Is the JTAG which is provided in uPSD3334D Testable. The thing is we are Programming the uPSD using the JTAG Interface Can we test the JTAG using some Scan Engine where we require the BoundaryScanDescription Files(BSDL).. Can we Perform Boundary Scan Test(BST) for the JTAG Compatible uPSD...

Thanks & Regards

Sharmash.D

joseph2399
Associate II
Posted on May 17, 2011 at 12:07

The uPSD as it is a stack die configuration is not 100% compatible with the JTAG for Boundary Scan spec. It can reside on the chain for In-System Programming purposes only, but must be placed in Bypass mode during boundary scan.