cancel
Showing results for 
Search instead for 
Did you mean: 

re-mapping the interrupts

babidesai123
Associate II
Posted on December 11, 2008 at 11:44

re-mapping the interrupts

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
babidesai123
Associate II
Posted on May 17, 2011 at 11:53

Hello,

Can anyone give me the clear picture of how the interrupt remapping is done?

According to data sheet of upsd3233 it's in program memory.

So, if secondary memory has been mapped as program space & primary as data space then once we program the primary as code memory in IAP & if start booting from primary.

Will those interrupt location will be automatically remapped?

If not then plz let me know what is the vector location of all int

(it's starts from 0000h in program memory) but it's primary or seconadry falsh?
anilwpatil
Associate II
Posted on May 17, 2011 at 11:53

Hi,

i am also got stuck into same problem of remapping interrupt after application downlaod via IAP. Can you help in this regards, i am using str731 and keil environment for my development.

Thanks and regards,

Anil