cancel
Showing results for 
Search instead for 
Did you mean: 

PSD854f2 - Security Bit

rchristopher
Associate II
Posted on February 19, 2007 at 12:02

PSD854f2 - Security Bit

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
rchristopher
Associate II
Posted on May 17, 2011 at 11:51

Hi,

I have an Infineon C515C and a PSD854F2 with IAP.

I am a little bit confused about the security bit: PSDSoft says:

Setting the security bit will block all access of the contents of the PSD from a JTAG or Conventional programming tool. This means that once the security bit is set, no programmer can read or copy the configuration or memory contents of the PSD. The only way to defeat the security bit is to erase the entire PSD

Do I understand correctly, that when this bit is set, I can still:

- IAP via RS232, but the flash cannot be read out with a JTAG tool

- do a full erase with PSDSoft, which resets this bit.

My confusion comes from p. 28 of the datasheet, which has two different tables, the table describing the security bit being named PSD/EE protection register. I don't have any EEPROM.

Regards, Ralph