cancel
Showing results for 
Search instead for 
Did you mean: 

Problems loading the monitor with the ST10Flasher tool

rcartarius9
Associate
Posted on January 13, 2008 at 16:45

Problems loading the monitor with the ST10Flasher tool

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
rcartarius9
Associate
Posted on December 05, 2007 at 10:24

Hi,

I have problems with the ST10Flasher tool. This tool seems not to work on all machines. I use an own hardware (with ST10F269) and I have some PCs which are not able to flash a new hex-file.

I allways get the message that it is not possible to load the monitor.

On other PCs I have no problems.

On some PCs it takes up to ten times until I succeed.

I want to know on what it depends on if the ST10Flasher works.

najoua
Associate II
Posted on January 10, 2008 at 12:41

Hello,

Could you please tell me which version of the ST10Flasher you are using and on which platform you are running it (2000, XP etc...)?

Best regards,

Najoua.

newsamo
Associate II
Posted on January 13, 2008 at 16:45

I have samo trouble....i read an hex file...and then when i try to rewrite it i get a file error...