2007-11-06 9:03 PM
2007-11-06 9:03 PM
Hallo,
I want to use the serial interface and i had used the code below (I use Tasking)but it did not work. can someone please help me. (XPEN, XASCEN, XMISCEN are set in the startup code) #include #include /*********************************************/ void xasc_init( void) { /* xasc interface in 8-bit mode, with no parity, no erroir checking , receiver enable */ XS1CON = 0x0011; /* XS1BG Fcpu = 40000000, SOBRS = 0*/ XS1BG = 0x81; /* xasc buffer transmit interrupt configuration */ XIR2SEL =0x2000; XP2IC = 0x0040 | ( 0x0005 << 2) | (0x0001); /* set port pins P8.7 -> Tx, P8.6 Rx */ XS1PORT |= 0x0010; _nop(); XS1PORT |= 0x0008; /* xasc interface enable */ XS1CONSET = 0x8000; } /**************************************/ interrupt( 0x42) void xasc_transmit(void) { static unsigned char index=0; static unsigned char Message[5] = ''Hello''; XIR2CLR = 0x0020; XS1TBUF = Message[index]; index++; if( index == 5 ) index = 0; } main() { xasc_init(); /* trigger the first transmission by setting the flag XIR1SEL*/ XIR2SET = 0x0020; XP2IR = 1; while(1); } [ This message was edited by: kerzingereric on 07-11-2007 10:46 ]