problem with GPIO internal Pull up
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-03-14 11:54 PM
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-03-13 9:38 PM
Posted on March 14, 2006 at 06:38
Hi,
I can't set the P0.10 gpio pull up internal resistor. I'm using the STR710 library and the following code: //set the P0.10 in pull up/ pull down weak input mode GPIO_CONFIG(GPIO0, 0x0400, GPIO_IPUPD_WP); //Set the pull up resistor GPIO_BITWRITE(GPIO0, 10, 1); NB : I'm using a raisonance evaluation card with a str712f microcontrollers. Thanks.Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-03-14 11:46 PM
Posted on March 15, 2006 at 08:46
P0.8 and P0.10 are ''true'' open drain rather than being push pull.
I put the question to ST about P0.8 and they indicated that the week pull up is NOT available on this pin (as part of it's 5V tolerance I believe). The doco does not advise that weak pull up is not available. Even after you move it to another pin be careful. If you use the library, when you change a different output pin on the same port you can change your pull ups to pull downs. This is because they do a read modify write on the port data register. When it is read it reads the INPUT state and when you write it back it sets the pull down polarity.Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2006-03-14 11:54 PM
Posted on March 15, 2006 at 08:54
thanks a lot for these informations.