cancel
Showing results for 
Search instead for 
Did you mean: 

PortB problem

luigi2
Associate II
Posted on June 01, 2005 at 12:59

PortB problem

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
luigi2
Associate II
Posted on May 17, 2011 at 12:07

Hello!

what is the difference whit the I/O port of MCU P1,P3,P4 and the I/O port OF PSD PortA, PortB,PortC, PortD

jdaniel
Associate II
Posted on May 17, 2011 at 12:07

There are pretty significant differences. The MCU ports (P1, P3, and P4) basically have the same electrical characteristics as the Intel 8032AH MCU. This means that they're TTL-compatible and not CMOS technology. The PSD ports ARE CMOS ports which means that have much higher Voh and lower Vol. Additionally, they're capable of sinking / sourcing far more current than the MCU ports. Finally, the PSD ports can interact with the programmable logic to automatically serve different functions (chip selects, etc.).