cancel
Showing results for 
Search instead for 
Did you mean: 

PLEASE!! *any* working examples for Hitex comStick??

dan1
Associate II
Posted on June 11, 2008 at 21:51

PLEASE!! *any* working examples for Hitex comStick??

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
dan1
Associate II
Posted on May 17, 2011 at 09:53

Other than the examples that actually come with the comStick itself??

This has been driving my nuts:

1. The Hitex examples *only* work with the version of toolchain that it comes with

(V4.0.3).

2. Their examples don't use gcc to call ld/as, they call these tools directly,

pathing to an unexpected path for the libraries.

3. If I try to change their code to call through gcc, I cannot make it find

the correct library path, no matter how many different places I specify the

path.

4. If I try any other GnuArm toolchain, I can never get the project to build.

I either get floating-point inconsistencies, interwork inconsistencies,

or other system functions not found (CodeSourcery).

I DESPERATELY need to find a simple project that builds with any of the standard tools (Yagarto would be a good choice), and can just simply toggle the status LED on the comStick board!!! (port 9 pin 0 or port 4 pin 1, where I also have an LED, which only Hitex is able to toggle!!).

Can anyone give any pointers for this??