cancel
Showing results for 
Search instead for 
Did you mean: 

Pin Number 44 Port Software Pull-down Solution??

kis75
Associate
Posted on July 11, 2007 at 16:14

Pin Number 44 Port Software Pull-down Solution??

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
kis75
Associate
Posted on July 11, 2007 at 05:58

Hello?

STR710FZ2, Pin Number 44, External Port Open Mistake (Data Sheet, I see Mistake)

A. Problem.

1. Centigrade 60 Over, CPU Shutdown(Lock-up) cycle Stop!

2. I Test Result, 44Pin Hardware Pull-down after Centigrade 60 Over Test Result No Problem'

B. The Present Time.

1. 10,000 EA Board SMD completed to Feild Running

C. Your Solution.

If your company solution? Only Software Solution.

Hardware Revision is My Company Big Impact.

(Hardware Port 44Pin Pull-down Solution not ok! )

Please, Only Software Solution result

Thanks, Good Bye :-[

[ This message was edited by: kiss on 11-07-2007 09:30 ]

________________

Attachments :

STR710FZ2_TQFP144_.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtO4&d=%2Fa%2F0X0000000aPG%2FtWPmuZT0VKqG6RjLw8SUJLYayXWZHXBe.u.Hw9.Lcow&asPdf=false
kleshov
Associate II
Posted on July 11, 2007 at 16:14

Sorry, but I think you are out of luck. The manual says:

DBGRQ. When high, the system requests the ARM7TDMI to unconditionally enter the debug state. This pin must be kept LOW when emulation features are not enabled.

It's a hardware problem, and I cannot see a possible software workaround.

- mike