cancel
Showing results for 
Search instead for 
Did you mean: 

PCB Design & Assembly files for STDES-30KWVRECT

Om1
Associate

Hello ST Team,  

 

I am working on the STDES-30KWVRECT Vienna PFC rectifier board and I need the following hardware resources:  

1. PCB design files (Gerber or Altium project)  

2. Assembly drawing with reference designators (for component placement)  

3. Any available footprint/library files related to this design  

 

This information will help me to reproduce the hardware accurately for research and prototyping purposes.  

 

If these files are subject to NDA (Non-Disclosure Agreement) or require additional steps to access, please let me know how I can proceed.  

 

Thank you very much for your support.  

 

Best regards,  

Omkar Swami  

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Om1, to the community!

For security reasons, no source code is made available for such high-power applications. Also, only the design documentation is available from STDES, it is not offered for sale.

You are welcome to get in touch with your local distributor or sales contact who will help you realise your project if the quantity is large enough.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Om1, to the community!

For security reasons, no source code is made available for such high-power applications. Also, only the design documentation is available from STDES, it is not offered for sale.

You are welcome to get in touch with your local distributor or sales contact who will help you realise your project if the quantity is large enough.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.