cancel
Showing results for 
Search instead for 
Did you mean: 

PB6 voltage level

gavin1
Associate II
Posted on January 31, 2007 at 11:18

PB6 voltage level

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
gavin1
Associate II
Posted on January 31, 2007 at 11:18

Dear All,

In an application I'm writing I'm having problems using PB.6 as a push-pull output. I get 1.7V without load on the output when I'm expecting 5V! This would not be a problem but when I try to drive a transistor with pin PB.6 there's not enough forward bias to turn the transistor on! Any Ideas anyone?

Hmmm. Have lifted some of the legs on the ST7 and it seems only some of them are outputting 5V when turned on.

Would the issue I describe be because the pins that I am using must be high sink in order to drive a transistor base?

[ This message was edited by: marco_bsl on 01-02-2007 11:28 ]

[ This message was edited by: marco_bsl on 01-02-2007 11:49 ]