cancel
Showing results for 
Search instead for 
Did you mean: 

OFDM over str9

gabriele2
Associate II
Posted on April 20, 2007 at 12:23

OFDM over str9

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
gabriele2
Associate II
Posted on May 17, 2011 at 09:39

I would like to know if some one have try to implements an OFDM modulation using for examples an STR9. I see that it can perform an 256Point FTT in about 200us.

I see also that this device have an 10Bits A2D with a convertion time of 1uS.Is possible in some way to increase the ''sensibility'' form 10bits to 12Bits?

sienickia
Associate
Posted on May 17, 2011 at 09:39

Actually, I've got the same problem. I'd like to control a robot using WLAN ieee 802.11 b. I know I have to modulate somehow signal from MAC unit though I don't know signal parameters. I would appreciate the answer if there's on the market any baseband processor (for OFDM modulation and signal conditioning) so that I could easily connect my STR912 to such baseband processor and then to ZIF transceiver.Are there such devices on the market? If not then how to enable STR912 to communicate through WLAN - (WiFi)?