cancel
Showing results for 
Search instead for 
Did you mean: 

Need help with STM32U5 and SPI

VSANGIL
Associate

Hi Folks:

I have this Riverdi board (RVT50HQSNWC00) with a STM32U5A9NJH6Q MCU.

I want to programming data transmission according to the image attached 

Im intent to use SPI but if any better option let me know

thanks in advance 

IMG-4286.jpg

 

 

1 REPLY 1
KDJEM.1
ST Employee

Hello @VSANGIL and welcome to the community;

 

I apologize for my late reply.

If I understood your question, is the RVT50HQSNWC00 supported by the SPI interface?

Could you please refer to RVT50HQSNWC00 display datasheet and check if the device supports the SPI protocol or not.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.