cancel
Showing results for 
Search instead for 
Did you mean: 

main VR OFF issue and power consumption of STDBY at V18bkp

shinnlin
Associate II
Posted on March 28, 2006 at 09:30

main VR OFF issue and power consumption of STDBY at V18bkp

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
shinnlin
Associate II
Posted on November 10, 2004 at 22:43

I have two more questions about power management.

1. as stated on page 75 of user manual v4, “the PLL is automatically disabled when….�

So, if we use our own external 1.8v source and turn off the Main VR,

that will cause PLL off and limit the max. operating frequency to 1 MHz ?

It doesn’t make sense to turn off the PLL if we use external 1.8v source..

2. If we use V18bkp for Standby mode voltage source with RTC on,

what's the power consumption measured at V18bkp under Standby mode ?

The power consumption listed in datasheet seems to be measured at V33 that is not what we want.

thanks for your help !

shinnlin
Associate II
Posted on November 15, 2004 at 02:41

Thanks, RISC !

If STR7's core is under power down, not in STDBY mode, which means we don't supply v33 to it but just provide V18bkp to keep RTC active, I'd like to know the power consumption of RTC.

Specifically speaking, I'd like to know how long it can last if we use a backup battery for RTC. So, I need the power consumption of RTC through V18bkp.

dmerchez9
Associate II
Posted on May 17, 2005 at 05:48

Hello everybody

I have the same question: what's the power consumption of standby at V18BKP?

shangdawei1
Associate II
Posted on March 28, 2006 at 09:30

Hello everybody

I have the same question: what's the power consumption of standby at V18BKP?

Can i use 3.3V battary to supply 1.8V for V18BKP pin and 3.3V for V33 pin when str71x is in STANDBY mode?