2024-06-02 8:09 PM
Dear ST Team:
We have E2PROM M24C64-WMN6P in our project, we checked from datasheet Page 20 & Page 25,there is a confusion need your help.Thanks
On Page 20, Table 12 shows Cbus load for I2C is 100pF max and 50ns max rise time,
While on Page 25,Table 19 showes we should follow I2C specification which mean Cbus up to 400pF, and rise time up to 300ns @400KHz
So which one should to follow? Pls confirm,Thanks
Best Regards
Lisa
Solved! Go to Solution.
2024-06-03 4:35 AM
Welcome @LisaXu, to the community!
Please don't get confused:
To answer your question: follow the parameters in table 19.
Hope that helps?
Regards
/Peter
2024-06-03 4:35 AM
Welcome @LisaXu, to the community!
Please don't get confused:
To answer your question: follow the parameters in table 19.
Hope that helps?
Regards
/Peter
2024-06-03 5:39 PM
Hi Peter:
Thanks for your clarification, And I will Follow Table 19.
Best Regards
Lisa