2025-08-21 1:33 PM
I want to do some testing and experimenting with the FSM features of the LSM6DSO. I have MEMS Studio downloaded, and I also downloaded the X-CUBE-MEMS1 expansion software package. I see on the documentation for X-CUBE-MEMS1 that the NUCLEO-L476RG was replaced with the NUCLEO-U575ZI-Q in November 2022. I also found X-CUBE-MEMS1-V4, but on the page, I cannot find a download link. I was wondering if someone could provide me the firmware for my setup, or some guidance on how I can get it working with MEMS Studio, so that I can play around with the FSM on the LSM6DSO.