cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L7CX Range Sigma Factor

Cafko
Associate

Hi, 

I am currently testing the VL53L7CX ToF sensor. During my evaluation, I came across the parameter "range sigma", but I could not fully understand what it actually represents.

In addition, while creating a correlation map, I noticed that the most influential feature affecting distance measurements is the range sigma value.

I would greatly appreciate it if anyone clarified what exactly "range sigma" indicates, and how the sensor calculates or measures this value. Can anyone enlight me?

Thanks

3 REPLIES 3
John_Kvam
Senior II

For all ST's time-of-flight devices, Sigma means he same as in your statistics class. 

The user guide say's:

Range sigma 128 x nb targets
programmed Millimeter Sigma estimator for the noise in the range estimate.

Which is NOT much help. 

But think of it this way. It's the distance - plus or minus - where 68% of all ranges would appear. 

So if you distance was 1 meter with a sigma of 3 - then if you took a lot of measurements 68% of them would be within 997 to 1003mm. 

But if your target returned too few photons, or if you were looking at a complex shape you could end up with a sigma quite a bit larger. 

But instead of looking into the math too deeply it just means lower is better.

And if you want to set a limit so you are warned when the sigma gets too high, Set that limit.

Instead of getting a 0 status value, you will an 'over sigma' return status. 

- john 

If this or any post solves your issue, please mark them as "Accept as Solution". It really helps the next guy.
And if you notice anything wrong do not hesitate to "Report Inappropriate Content".
I am a recently retired ST Employee. My former username was John E KVAM.

Firstly, I apologize for my late response.

When I first started using this sensor, I had the same thought I assumed this value represented one sigma, which corresponds to the 68% region in a Gaussian distribution. However, after collecting more data, I realized that there is no meaningful relationship between the distance standard deviation and the range sigma value. I then started searching and found that it might represent the SNR in the area. But if that is the case, the unit in the datasheet should be mm² rather than mm. So according to my tests i dont think this is not the gassian sigma value of distance. 
but when i check the range sigma's and distance correlation it is highly effective on distance. but i could not figure what it is.
And also i collect my data from a flat wall to not include other distribution errors. 

I was afraid you might actually do the math. 

Some of the ToF sensors actually use a statistical process to get the range.  (VL53L0, L1CX, and the L4CD). But the others use Histograms. And with histograms there is no real sigma. 

But the early customers liked sigma - and it was decided to return one. 

But clearly, it's not something that just falls out of the algorithm. 

So, I think the best that can be said is that the sigma returned by the histogram parts is a guess at the sigma. 

A small sigma indicates a really confident range value, and a large sigma means there is something about the range that is suspect. 

Now that I've retired, I find it really hard to use ST and not 'we'.

- john

If this or any post solves your issue, please mark them as "Accept as Solution". It really helps the next guy.
And if you notice anything wrong do not hesitate to "Report Inappropriate Content".
I am a recently retired ST Employee. My former username was John E KVAM.