cancel
Showing results for 
Search instead for 
Did you mean: 

Load and Debug a Programm in external RAM or FLASH

ahennig9
Associate
Posted on August 26, 2004 at 11:21

Load and Debug a Programm in external RAM or FLASH

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ahennig9
Associate
Posted on August 26, 2004 at 09:41

Hello Guys

I use the Demoboard, RV JTAG-IF and Software all from ST

till our own Hardware ist available.

I think our Softwareprojekt ist bigger as 256k in future

Is it possible to debug Software in External FLASH or SRAM

in Bootmode EXTMEM mapped at 0h via ARM JTAG/Realview

How can I load my Software via Jtag in Ext.FLASH.

I found no ready to use Tool in REALView Debugger.

Why the debugging in in the internal FLASH is different to

debugging in internal RAM per examble ''Brakepoints''.

what shall i do if my programm is bigger as 64k to

run debugging komplete in internal RAM.

What shall i do if my programm is bigger as 256k to

run debugging komplete in internal Flash

shall i debugg small parts of my software only in Bootmode

RAM mapped at 0h. and then Link whole Projekt with all parts and

Burn it via ext. Prommer/Flasher Soft or Hardware an Test it

Komplete like Methode ''Try and Error''

This is my knownmend at this time.

Please Post me your opinion.

I speak crasy english sorry but very good german.

AndyHennig