cancel
Showing results for 
Search instead for 
Did you mean: 

KickStart IAR release configuration

tim11
Associate II
Posted on May 29, 2006 at 13:33

KickStart IAR release configuration

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
tim11
Associate II
Posted on May 26, 2006 at 18:41

I have a small application that I have developed using IAR KickStart and now would like to compile it optimized/released. How do you configure the IDE so it will download the .elf output into flash using the J-Link USB-JTAG tool? I have tried many things including setting up the release with Debugger set to J-Link but the IDE crashes when it gets near the end of programming the STR711.

[ This message was edited by: tim35ca on 29-05-2006 06:27 ]

tim11
Associate II
Posted on May 29, 2006 at 13:33

So what are the implications of running a d79 file on a STR711 based board as a final application, i.e. no J-Link debugger attached? Or am I going to have to buy a full blown IAR-EWB to deploy this small project.