2003-11-13 9:08 AM
2003-11-07 1:00 AM
Does anybody know if I can disable the IDE bus and use only the ISA bus.
If that´s possible, is there a way to generate internally the chip selects when the IDE Bus is disabled? The fact is that I cannot use the IDE bus but I need to access a Hard drive. I could implement it on the ISA Bus, but i need the chip select signals. Unfortunatelly I don´t have enough room to place any kind of decoder. If anyone has a clue... Thanks.2003-11-13 9:08 AM
You message misses details for an answer from the people:
- what CPU are you using? - ISA and IDE almost share the same lines, why can't you use the IDE? - can your BIOS allow you to use a USB hard drive?