cancel
Showing results for 
Search instead for 
Did you mean: 

Invalid core Id. (0)

ricardo2399
Associate II
Posted on September 05, 2008 at 08:39

Invalid core Id. (0)

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
amira1
Associate II
Posted on May 17, 2011 at 09:55

Hello ricardo.marinheiro,

Did you measure the IDD(1.8V) and IDDQ(3.3V) in your board? It can be a hardware problem. Or try to erase the flash and try to load the program again.

Please do these tests and let me know.

Best regards,

mirou.

ricardo2399
Associate II
Posted on May 17, 2011 at 09:55

hi everyone

I'm complitely blocked in here... i can´t do anything!!!

Fri Aug 22 13:41:50 2008: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 5.0 Kickstart\ARM\config\flashloader\ST\FlashSTR91x.mac

Fri Aug 22 13:41:50 2008: DLL version: V3.90b, compiled Aug 21 2008 14:51:23

Fri Aug 22 13:41:50 2008: Firmware: J-Link compiled Jul 30 2008 11:24:37 ARM Rev.5

Fri Aug 22 13:41:50 2008: JTAG speed is using adaptive clocking (RTCK signal)

Fri Aug 22 13:41:50 2008: Initial reset was performed

Fri Aug 22 13:41:50 2008: TotalIRLen = ?, IRPrint = 0x..00000000000000000000000000000000

Fri Aug 22 13:41:52 2008: Fatal error: Invalid core Id. (0)

have you ever seen this?...

can anyone help with this??

thank you

:-[

ricardo2399
Associate II
Posted on May 17, 2011 at 09:55

Hi

The problem was BootLoader became all messed up and i just used a SEEGER tool to upload it again to his place, and all went well.

By saying that BootLoader was a mess, it was what i assumed once the j-Link couldn't sync with ARM becouse it was no RTC clock to do it.

Hope it help =)