cancel
Showing results for 
Search instead for 
Did you mean: 

Sw delay

sr_shinde
Associate II
Posted on September 23, 2008 at 02:47

Sw delay

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
sr_shinde
Associate II
Posted on May 17, 2011 at 09:55

Hi all ,

For S/W delay i just wrote For loop of Multiple of (96000 * 10000)

But It gives delay in just microseconds.I am using Ride Simulator.

PLL is 96Mhz.

Also if anybody has Timer Interrupt Configured for 1ms please send me.

Because i am not getting exact delay observed on CRO.

Please Reply

Regards

Sai

matthew239955_stm1
Associate II
Posted on May 17, 2011 at 09:55

The timer reset behavior is not intuitive. See this post for details:

http://www.st.com/mcu/forums-cat-7126-21.html

Matt

sr_shinde
Associate II
Posted on May 17, 2011 at 09:55

Thanks Matt

What about S/w delay.

Regards

Sai

matthew239955_stm1
Associate II
Posted on May 17, 2011 at 09:55

Sorry, I'm confused about your question.

When you say S/W delay, do you mean a simple loop or do you mean configuring the timer to interrupt at a given delay?

If you mean a loop, what exactly is your question?

And if you mean a timer interrupt, please post your code, expected behavior, and observed behavior so the forum can have a better idea what your problem is.

Matt

sr_shinde
Associate II
Posted on May 17, 2011 at 09:55

Hi all,

By s/w delay I mean to say simple for loop.

Clock configuration done is as follows:

/*wait state insertion: This function should be executed from

SRAM when*/

/*booting from bank1 to avoid Read-While-Write from the same Bank.*/

FMI_Config (FMI_READ_WAIT_STATE_2, FMI_WRITE_WAIT_STATE_0,FMI_PWD_ENABLE,

FMI_LVD_ENABLE, FMI_FREQ_HIGH);/*Insert 2 Wait States for

read*/

SCU_PLLFactorsConfig (192, 25, 2); /* PLL factors Configuration based

on*/ /* a OSC/Crystal value = 25 MHz*/

SCU_PLLCmd (ENABLE); /* PLL Enable and wait for Locking*/

SCU_RCLKDivisorConfig (SCU_RCLK_Div1); /* RCLK @96Mhz */

SCU_HCLKDivisorConfig (SCU_HCLK_Div1); /* AHB @96Mhz */

SCU_FMICLKDivisorConfig (SCU_FMICLK_Div1);/* FMI @96Mhz */

SCU_PCLKDivisorConfig (SCU_PCLK_Div2); /* APB @48Mhz */

SCU_MCLKSourceConfig (SCU_MCLK_PLL); /* MCLK @96Mhz */

Delay Function:

// ms delay

void Delay(unsigned int uint_TimeDelay)

{

unsigned int l_uintdelay1, l_uintdelay2;

for (l_uintdelay2 = 0; l_uintdelay2 < uint_TimeDelay; l_uintdelay2++)

{

//approx: 96000 instruction execution time (at 96 MHz MCLK) = 1ms

minimum

for (l_uintdelay1 = 0;l_uintdelay1

for (l_uintdelay1 = 0;l_uintdelay1

}

}

Delay used in application:

while(1)

{

GPIO_WriteBit(GPIO9,GPIO_Pin_3,Bit_RESET);

Delay(1);

GPIO_WriteBit(GPIO9,GPIO_Pin_3,Bit_SET);

Delay(1);

}

Expected Waveform (GPIO9.3):

OFF time: 1 ms min

ON time: 1 ms min

Waveform observed on Oscilloscope (GPIO9.3):

OFF time: 1 us

ON time: 1.36 us

I am using RIDE7 debugger.Crystal used is of 25MHz.So delay should be more than the expected but how it can be less than the expected?

Regards

Sai

daniel8
Associate II
Posted on May 17, 2011 at 09:55

Define your variables in your delay loop as volatile - that way the compiler wont optimize them out. If you are getting 1us times, then most likely that is whats happening.

sr_shinde
Associate II
Posted on May 17, 2011 at 09:55

Thanks for Reply

Now I am using timer for delay.

But i will definitly use for loop with ''nop'' for small time delay

Regards

Sai

dhoyen
Associate II
Posted on May 17, 2011 at 09:55

Hi,

I had this problem :

How to realise a delay..

and in fact, he doesn't work with a simple ''for'' loop :

Compiler optimization, i think detect your ''for'' loop empty,

and jump directly to the following line of code (TBC).

 

Can i suggest you to add this line just in your loop for :

 

and will solve (i think) your problem

 

 

should be :

 

 

for (i=0;i

 

{

 

asm volatile ( ''NOP'' );

 

}

 

But keep in mind, it's a lot of CPU cycle lost here... A timer is really better especialy for a long periode like 1msec

Regards

Damien

[ This message was edited by: dhoyen on 12-09-2008 10:32 ]

[ This message was edited by: dhoyen on 12-09-2008 10:34 ]