cancel
Showing results for 
Search instead for 
Did you mean: 

Interupt Code in SRAM Keil uVision

gumbi
Associate
Posted on December 07, 2006 at 04:37

Interupt Code in SRAM Keil uVision

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
gumbi
Associate
Posted on May 17, 2011 at 09:34

Hi,

i have made a short programm using interrupts an SSP. I have implemented SSP Data communication controlled by DMA in an interrupt function.

Now i have analyzed the timing. As a result the interrupt function need to much time until thhe code in the function is called. Is it possible to store this inerrupt code in the SRAM? the flash only works with the half operating frequency (48MHz). The SRAM should be much faster.

Best regards

Frank